Log in with YubiKey
Use this procedure to log in to Power Operation using a YubiKey and a one-time password.
Prerequisites:
The YubiKey is programmed and associated with a user in Power Operation, and the YubiKey is enabled.
To log into the system using YubiKey:
- Insert the programmed YubiKey into a USB port of the Power Operation server.
- Launch Power Operation Runtime, or access runtime using a remote Web Client.
- Run the project you want to view.
- In the upper right corner of the Startup screen, click Login.
- In the Power Operation Studio login screen, enter your name and password and then click OK.
- Press the button on the YubiKey.
The One-time Password screen appears.
The one-time password is generated. The key and software communicate behind the scenes to verify the uniqueness of the one-time password and to click OK.
You can start using Power Operation Runtime.